Industrial Automation & Control

Industry 4.0 is digitising and revolutionising manufacturing. By combining the Industry 4.0 models with advanced analytics, Artificial Intelligence (AI) and Industrial Internet of Things (IIoT), we can introduce speed and precision to a wide range of factory operations, enhancing productivity and reliability

MOLEX
ABB
EATON
TRINAMIC / ANALOG DEVICES
HONEYWELL
MITSUBISHI
OMEGA
OMRON
PHOENIX CONTACT
SCHNEIDER ELECTRIC
SIEMENS
FLUKE
3M
WERA
KNIPEX
RASPBERRY PI
ARDUINO PRO
KUNBUS
DFROBOT
WITTRA
BEAGLEBOARD

By combining the advantage of Industry 4.0 models with advanced data analytics, Artificial Intelligence (AI) and Industrial Internet of Things (IIoT) we can introduce speed and precision to a wide range of factory operations, enhancing productivity and reliability. The rapid evolution of this technology and its integration across the enterprise is reshaping the ways manufacturers operate and produce high-quality goods.

Benefits include:

  • Reduced periodic and manual checking
  • Increased productivity
  • Reduced production cost
  • Improved product quality
  • Increased flexibility
  • Improved safety

Outlined below are three main levels of industrial automation applications:

Level 1 - Supervisor Level:

Mainly PC-based systems, such as industrial PCs (rack-mounted and panel) equipped with supplier-specific industrial process-control software for process parameterization and visualization. The intercommunication is based on a Gbit LAN or higher bandwidth backbone or Wireless topologies (WLAN). To avoid data loss and for safety reasons, Uninterruptable Power Supplies (UPS) are installed.

Core Components: Industrial PC, Panel PC, HMI, WLAN

Level 2 - Control Level:

This is the automation systems level where automation programs are executed. Systems on this level require high real-time capability and are based on a special controller architecture with its own proprietary OS running on it. High real-time compliant intercommunication bus protocols (according to IEEE 1588) are essential here.

Core Components: PLCs, HMI, Field Bus (CAN, EtherCAT, Profibus etc ), WLAN, Safety (SIL).

Level 3 - Field Level:

This level includes all terminal equipment, such as sensors and actuators collaborating with a peripheral PLC or remote I/O system, offering pre-procession of the collected data and communication to the main PLC via field bus.

Core Components: Micro PLC, Motor Control, Industrial Sensors, Actuator Drivers, Relays, Switches, Wireless Control (RFID, wireless sensor networks using IEEE 802.15.4 topology)

Mostrar mais

We are Industrial, Motor Control, Sensors, PLCs, Controllers & SBCs

Industrial smart Energy Efficiency Solutions

Industrial smart Energy Efficiency Solutions

Motors & motor controllers, VSF Drivers, PLCs, Power, Sensors

Smart Maintenance & Repairs

Smart Maintenance & Repairs

Reduce costs, increase up-time

Smart Sensor Solutions for IIoT

Smart Sensor Solutions for IIoT

Track. Control. Improve Efficiency. Reduce Cost.

Edge Computing Transformation

Edge Computing Transformation

Sensors, PLCs, HMIs, SBCs

Featured Content

Article

Integrating Single Board Computers for Machine Vision in Industrial AutomationExplore the power of Single Board Computers (SBCs) in revolutionizing industrial automation through Machine Vision. Enhance efficiency, reduce downtime, and embrace Industry 4.0 with our insightful guide.

Article

Robotics and AI Integration: Transforming Industrial AutomationDiscover how the integration between robotics and artificial intelligence reshapes industries, challenges norms, and propels the future.

How-to

How Industry 4.0 is driving HMI technologyIn an industrial context, a human machine interface (HMI) allows an operator to interact with their machine or process. It shows the machine’s status, and allows the operator to input commands.

Blog

Integration of Edge computing in PACs and PLCsLearn the essential differences between PLCs and PACs, the breadth of communication, and the advantages of using smart PLCs and PACs to create a smart factory.

How-to

How infrared cameras (IR) help in condition monitoringA thermographic camera (Infrared imaging or thermal camera) uses infrared radiation to detect objects. Infrared imaging plays an essential function in predictive maintenance. The cameras monitor plant machinery or equipment to create thermal images that reveal hot spots. These hot spots help detect future malfunctions, overheating, machinery or facilities damage, and personnel injury. Repairs or maintenance can be performed at the safest and most cost-effectively.

Article

Top 10 industrial robot sensors for enhanced automationExplore the top 10 industrial robot sensors that enhance automation, improve precision, reduce errors and boost manufacturing efficiency.

Article

Analog Devices: IO-Link® - A Pivotal technology for smart Industrial AutomationIO-Link is a standardized technology regulating how sensors and actuators in industrial systems interact with a controller, allowing bidirectional communication and configuration between a sensor and a controller.

Article

Raspberry Pi in industrial automationExplore Raspberry Pi's versatile applications in industrial automation, from data acquisition to edge computing, and learn about the compact Compute Module for commercial use