Informação do produto
Descrição geral do produto
942 is a Pi Dish for Raspberry Pi, its a way to attach a Raspberry Pi computer to a plastic 'dish' with a full sized breadboard. Designed carefully to make it as easy as possible to attach and detach the Pi. Since the Pi computer does not have any mounting holes, we use these nifty plastic edge 'grabbers', they are incredibly strong but will not damage the Pi circuit board. There are two ways to mount the Pi on to the plate. one if user want to use the HDMI output primarily and one if user plane to use the composite output. Next to the Pi is a spot for a full sized breadboard, plenty of space for project even if using an Cobbler breakout helper. Also included 4 rubber bumpers to attach to the bottom.
Aplicações
Hobby & Education
Conteúdo
Laser cut acrylic plate, Mounting hardware for Pi with clips and screws, Four bumpers, Clear breadboard.
Especificações Técnicas
Pi Dish
HATs - Interface
Raspberry Pi
To Be Advised
Documentação técnica (1)
Legislação e Ambiente
Certificado de conformidade do produto