Press Releases

Newark launches full-featured SoC FPGA Lark Board

Development kit based on Altera’s ARM-based Cyclone V SoC available exclusively through Newark

November 10, 2014 – CHICAGO – Newark has announced the launch of the Lark Board, a high-performance development board based on Altera’s Cyclone® V SoC. The Lark Board is designed for development of high-volume applications including automotive, medical equipment, video surveillance and industrial control.

“The launch of the Lark Board enables developers to efficiently utilize the advantages of Cyclone V SoC architecture, density and performance, offering a full-featured and powerful development platform for embedded system design and development,” said Joerg Bertholdt, Director, Embedded Software Marketing and Planning at Altera.

The Lark Board features a 5CSXFC6D6 SoC FPGA, the largest SoC device in the Cyclone V SX family. This device integrates an FPGA and ARM-based dual-core Hard Processor System (HPS) that operates at speeds up to 800 MHz and is coupled together through an AXI high-speed interconnect backbone to the FPGA fabric. A single monolithic device combines the performance and power savings of hard intellectual property with the flexibility of programmable logic.

“We are delighted with the opportunity to develop the Lark Board, which highlights Altera’s leadership in programmable logic solutions and our design capabilities in embedded products,” said David Shen, Chief Technology Officer at Premier Farnell. “Engineers will appreciate the power, speed and flexibility this industry-leading SoC development kit provides at a price point not normally seen for full-featured, FPGA-based evaluation boards.”

The Lark Board provides 1GB DDR3 SDRAM to each of the HPS and FPGA as well as 4GB eMMC Flash and a Transflash card slot for mass storage. The Lark Board features several standard I/O interfaces including PCI Express, Gigabit Ethernet, USB2.0 Host ports, UART, JTAG, and 3G SDI. The combination of HDMI, VGA and LCD screen support gives the Lark Board a competitive advantage; moreover, it supports VGA display up to 1920x1080 and 1080 HDMI digital output making it ideal for video intensive applications. It also features a 30-pin digital camera connector ideal for surveillance type applications.

Get a tour of the Larkboard on Dec. 2, 2014 by joining element14’s webinar, “Developing Advanced Embedded Systems with Altera Cyclone V SoC and element14 Lark board” during which Todd Koelling from Altera and Craig Stiegman from element14 will discuss how its flexible architecture allows multiple configuration options and customizable hardware designs to be implemented. Registration is free and open to all element14 Community members.

The Lark Board also integrates a 12-bit high-speed and a dual-channel 3.3GHz RF/IF differential amplifier alongside a 12-bit 105MSPS high-accuracy ADC to enable analog signal amplification, filtering and sampling. The Lark Board uses an Altera Enpirion® power solution to provide a stable and efficient output for all the Cyclone V SoC’s power rails.

A USB Blaster II has been integrated on the Lark Board to increase the efficiency of FPGA debugging. The onboard USB Blaster supports Quartus® II and ARM DS-5 development environments. The Lark Board comes pre-installed with Yocto, an embedded distribution of Linux with other Linux distributions available to download online.

The Lark Board is available exclusively for $940 from Newark in North America, Farnell element14 in Europe and element14 in Asia Pacific. Data sheets and application notes can be found on the product pages together with a range of associated accessories and 24/5 live tech support is available for any queries. This new development board is the latest in Newark’s diverse portfolio ranging from starter kits to complete development boards, including the newest releases and exclusive bundles from the largest range of development kits available globally from one single source – the element14 Design Center.

-End-

About the Premier Farnell Group

Premier Farnell plc (LSE:pfl) is a global leader in high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. It trades as Farnell element14 in Europe, Newark in North America and element14 across Asia Pacific. With sales last year of £968m, the Group is supported by a global supply chain of more than 3,500 suppliers and an inventory profile developed to anticipate and meet its customers’ needs.

Premier Farnell works with key strategic suppliers to bring to market development kits in a variety of applications, enabling it to support the customer from design concept through to production.

The latest products, software, services and solutions from trusted supplier partners are all available through 43 local language transactional websites, with customer support provided by degreed engineers. The element14 Community allows buyers and engineers to access a wide range of independent technical information, tools and the latest resources.

For news updates from Premier Farnell and element14 visit:

Premier Farnell News Centre – www.premierfarnell.com/media-centre
Twitter – @element14news; @element14
YouTube – element14
Facebook – facebook.com/element14page
Email: pressoffice@premierfarnell.com

Premier Farnell Key facts

  • Operations in 36 different countries
  • More than 4,300 employees
  • More than 3,500 leading suppliers
  • More than 500,000 products stocked with access to over four million more on demand
  • Leaders in providing information on REACH, Conflict Minerals and EU RoHS legislation

For more information visit the website at Premier Farnell.

Global Contact:
Ken Leitch
Global Head of PR
Tel: +44 207 851 4145
Email: kleitch@premierfarnell.com

Global PR Agency:
Darren Willsher/Andrew Hill
EML Wildfire
Tel: +44 208 408 8000
Email: element14@emlwildfire.com  

European Contact:
Jen Cooke
PR Manager, Europe and Global
Tel: +44 113 279 0101
Email: jcooke@premierfarnell.com 

APAC Contact:
Christina Loh
PR Manager, APAC
Tel: + 65 6671 8769
Email: cloh@element14.com

North America Contact:
William Polk
PR and Social Media manager
Tel: +1 773 907 5199
Email: wpolk@newark.com