Press Releases

Take Control with Exclusive PiFace™ and SHIM Accessories for the Raspberry Pi from Newark

October 2, 2014CHICAGONewark and the team that designed the PiFace™ have launched a new series of exclusive Raspberry Pi accessories and the PiFace Digital 2 – an update to the popular PiFace Digital Control & Display.

Compatible with the recently launched Raspberry Pi model B+, the PiFace™ Digital 2 helps to sense and control real world applications. It is a simple and easy way to connect switches, lights, motors and more to the Raspberry Pi, allowing PiFace to interface with the world around it. The PiFace Digital 2 includes components like relays, switches, and digital and analog I/O that will allow it to be controlled by the Raspberry Pi board.

Going portable with PiFace Control and Display 2 means there is no need for a monitor, keyboard or mouse. It includes a character display and controls the Raspberry Pi with onboard buttons or with an IR remote control. The PiFace Control and Display 2 is ideal for Xbox Media Center (XBMC) servers, Internet radios or in other Raspberry Pi applications, and an improved LCDproc open source software keeps track of the system’s performance.

The SHIM RTC (Real Time Clock) is the new accessory from PiFace which adds additional functionality without sacrificing Raspberry Pi GPIO. It is achieved with a uniquely designed thin layer PCB and pin-through holes, enabling it to sit on top of the Raspberry Pi, and has enough space for additional add-on accessories. The SHIM accessories also allow users to add on an RTC clock and extend Raspberry Pi GPIOs.

SHIM RTC means the Pi can keep track of the current time with accuracy without using up the GPIO header, an easy plug-and-play integration and development tool for designs and applications requiring timestamps. A back-up battery can also be used to ensure on-going timekeeping in power-down situations.

The SHIM Adapter is a Raspberry Pi GPIO extender, making it easy to connect additional add-on accessories, work with breadboards, attach wires or easily access pin testing all at the same time. With one set of holes placed over the Raspberry Pi headers the other set of holes on the SHIM Adapter can accommodate header pins and wires to support the users’ application without covering up the header pins for additional add on boards.

For more information on the accessories and to buy PiFace Digital 2, visit www.newark.com, and visit www.element14.com to access a library of Pi Projects that will help users get started.

-End-

About the Premier Farnell Group

Premier Farnell plc (LSE:pfl) is a global leader in high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. It trades as Farnell element14 in Europe, Newark in North America and element14 across Asia Pacific. With sales last year of £968m, the Group is supported by a global supply chain of more than 3,500 suppliers and an inventory profile developed to anticipate and meet its customers’ needs.

Premier Farnell works with key strategic suppliers to bring to market development kits in a variety of applications, enabling it to support the customer from design concept through to production.

The latest products, software, services and solutions from trusted supplier partners are all available through 43 local language transactional websites, with customer support provided by degreed engineers. The element14 Community allows buyers and engineers to access a wide range of independent technical information, tools and the latest resources.

For news updates from Premier Farnell and element14 visit:

Premier Farnell News Centrewww.premierfarnell.com/media-centre
Twitter@element14news; @element14
YouTubeelement14
Facebookfacebook.com/element14page
Email: pressoffice@premierfarnell.com

Premier Farnell Key facts

  • Operations in 36 different countries
  • More than 4,300 employees
  • More than 3,500 leading suppliers
  • More than 500,000 products stocked with access to over four million more on demand
  • Leaders in providing information on REACH, Conflict Minerals and EU RoHS legislation

For more information visit the website at Premier Farnell.

Global Contact:
Ken Leitch
Global Head of PR
Tel: +44 207 851 4145
Email: kleitch@premierfarnell.com

Global PR Agency:
Darren Willsher/Andrew Hill
EML Wildfire
Tel: +44 208 408 8000
Email: element14@emlwildfire.com  

European Contact:
Jen Cooke
PR Manager, Europe and Global
Tel: +44 113 279 0101
Email: jcooke@premierfarnell.com 

APAC Contact:
Christina Loh
PR Manager, APAC
Tel: + 65 6671 8769
Email: cloh@element14.com

North America Contact:
William Polk
PR and Social Media manager
Tel: +1 773 907 5199
Email: wpolk@newark.com