0
0 elementos$0.00

ROHM 4th Generation SiC MOSFETs – Application Benefits & Efficiency Gains

This article describes an experimental test using a step-down DC-DC converter with 500V input voltage and 7kW power, a simulated running test using an EV traction inverter with 800V input and 100kW, and an experimental test using a Totem-pole PFC circuit.

ROHM has released the 4th generation of Silicon Carbide (SiC) MOSFETs. It has achieved a 40% reduction in on-resistance and a 50% reduction in switching loss compared to the 3rd generation.

Key takeaways

  • Lower switching losses (Eon/Eoff) enable higher switching frequency and power density.
  • Reduced conduction losses via optimised RDS(on) at operating temperature.
  • Improved transient performance (dv/dt, di/dt) with stable gate-drive behaviour.
  • Thermal headroom can allow smaller heatsinks in many designs.

Browse ROHM SiC MOSFETs

 

This article describes an experimental test using a step-down DC-DC converter with 500V input voltage and 7kW power, a simulated running test using an EV traction inverter with 800V input and 100kW, and an experimental test using a Totem-pole PFC circuit.

However, as the world is currently strengthening its efforts to protect the global environment, simply improving comfort will not be enough to gain acceptance in the global market. In the future, in addition to improving convenience, it will become increasingly important to reduce energy loss and use it effectively.

The key point to focus on is power conversion. In all the above-mentioned applications, power is supplied from the power grid, batteries, solar power generation systems, etc., and converted to the optimal voltage for effective use. To reduce energy loss and increase power conversion efficiency, SiC power semiconductors are currently attracting attention for their ability to operate at high frequency, high voltage and high current density with low energy loss. ROHM has already commercialized SiC power semiconductors, which are used in a variety of applications.

Application examples

Applications where SiC MOSFETs are deployed across EV, ESS and industrial power stages.

Figure 1. Application examples

ROHM's 4th Generation SiC MOSFETs build upon the trench gate structure introduced in the 3rd generation, delivering significant performance improvements:

  • ~40% reduction in on-resistance
  • ~50% lower switching loss
  • High-speed switching even at elevated voltages and power levels

This evolution is shown in the trend of normalized on-resistance (Ron-A: on-resistance per unit area) shown in Figure 2.

Trend graph of normalized on-resistance

Figure 2. Trend graph of normalized on-resistance

4th-gen SiC improves the trench trade-off, reducing normalized on-resistance versus prior generation.

In contrast to the 3rd Generation SiC MOSFETs, the 4th generation offer improved switching speed, which contributes significantly to lower switching losses. Figure 3(a) shows the block diagram of the buck converter and Figure 3(b) shows the general switching waveforms of the converter.

Block diagram of the buck converter (Figure 3a) and the general switching waveforms of the converter (Figure 3b).

Figure 3. Block diagram of the buck converter (Figure 3a) and the general switching waveforms of the converter (Figure 3b).

Buck converter block and typical switching waveforms used to illustrate loss components.

As shown in Figure 3(b), power device losses in a converter consist of switching losses, conduction losses, body diode losses, recovery losses, and Coss losses. (Coss loss is omitted from the figure because it is small.)

As for switching loss, it is generally described in the datasheet as energy per Eon and Eoff pulse, which is a useful for loss estimation in the initial design stage. In detailed design, it is necessary to strictly determine the power dissipation at high voltage input and high frequency. The gate driving circuitry has a large impact in the device losses, so optimizing the gate drive design is necessary to take advantage of the high-speed switching characteristics of SiC devices.

Design notes

  • Gate drive: set Rg to balance EMI and switching speed; validate with a double-pulse test.
  • Layout: minimise loop inductance; keep high di/dt paths tight; use Kelvin source when available.
  • Thermal: size the heatsink for worst-case operation and monitor junction temperature.

Experimental Verification of DC-DC Converter

In order to confirm previous analysis, the 4th Generation SiC MOSFETs was incorporated into a step-down DC-DC converter with the following specifications and verified it experimentally with an evaluation board (table 1).

Figure 4 shows (a) the DC-DC converter circuit and (b) the evaluation board for the 4th Generation SiC MOSFETs used in the half-bridge section with built-in decoupling capacitor. The inductor L, output capacitor Co, and input bulk capacitor are external.

Table 1. Specifications of DC-DC Converters and SiC Device

Vin500V
Vo250V
Po7kW
fsw50kHz
L500uH
Rg_ext3.3ohm
4th generation SiC MOSFETsSCT4036KR 1200V/36mΩ
3rd generation SiC MOSFETs (as a reference)SCT3040KR 1200V/40mΩ
DC-DC converter block diagram for test and 4th generation SiC MOSFET EVK

Figure 4. DC-DC converter block diagram for test and 4th generation SiC MOSFET EVK.

Test converter diagram and evaluation board with 4th-gen SiC half-bridge and decoupling.

Figure 5 displays the VGS, VDS, and ID waveforms at 50 kHz during turn-on and turn-off. The turn-on waveform is enlarged on the left. From the waveform observation, we can see that the turn-on rise time Trise is about 20ns, which is very fast. Figure 6 shows the measurement results of efficiency and power dissipation of this DC-DC converter as well as the efficiency and loss of the DC-DC converter. At light loads (around 1kW), the low switching loss, which is a characteristic of the 4th generation SiC MOSFET, is presented.

Observed switching waveforms (500Vin, 250Vo/20A(5kW), 50kHz)

Figure 5. Observed switching waveforms (500Vin, 250Vo/20A(5kW), 50kHz)

Fast turn-on; measured Trise ≈ 20 ns at 50 kHz operating point.

Measured efficiency and losses (500Vin, 250Vo/7kW)

Figure 6. Measured efficiency and losses (500Vin, 250Vo/7kW)

Efficiency and loss results; 4th-gen SiC shows clear benefits at light load.

EV Application

There are various types of EVs, such as BEVs, HEVs, PHEVs, and series HEVs, with different power architectures for different applications. Among them, the power architecture of BEVs with 400V or 800V battery voltage supporting bi-directional and fast charging has been attracting attention recently.

Where 4th-gen SiC helps most

  • EV DC fast charging (high-frequency PFC/LLC stages).
  • Energy storage systems (bidirectional inverters).
  • Industrial drives (efficiency gains at partial load).

Compare ROHM SiC options

Figure 7 illustrates a block diagram of the BEV power architecture as an example: the OBC (On-Board Charger) is a hot topic topology with bi-directional Totem-pole PFC and bi-directional CLLC (Symmetric LLC), assuming V2G (Vehicle To Grid). From the output of this OBC, power is supplied to the auxiliary DC-DC converter, the battery, the boost converter to the inverter and the motor traction inverter.

An example of BEV power architecture

Figure 7. An example of BEV power architecture

Example BEV architecture with bidirectional Totem-pole PFC and CLLC stages.

Simulated driving test with traction inverter

As the integration of mechanical and electrical components (motors, reduction gears, and inverters) continues to progress, the importance of reducing losses to achieve high voltage, high output, compact, and lightweight inverters is increasing. This is because it directly affects the cost performance of EVs.

As shown in Figure 8, the traction inverter converts the DC power provided by the battery into 3-phase AC power to drive the motor in the powertrain. The three-phase AC waveform is set by a signal wave (reference sine wave) with a frequency synchronized with the motor speed, and a triangular wave (modulation wave) with a carrier frequency that determines the switching frequency. The voltage supplied to the motor is determined by changing the levels of the 3-phase AC and triangular waves when generating the PWM signal.

Inverter circuit configuration and drive signal

Figure 8. Inverter circuit configuration and drive signal

Traction inverter configuration and PWM reference/carrier signals.

Motor test bench environment

Table 2 shows the main specifications of the SiC devices installed in the motor test bench and the DUT inverter. The DUT inverter consists of a 2-in-1 power module with a 4th generation SiC MOSFET bare chip.

Table 2. Main specifications of motor test bench and test inverter

DC power supplycapacity100kW
Output voltage range0 to 850V
Output current range± 500A
Test motorTypePMSM
Rated output100kW
Maximum torque (1 minute)350Nm
Cooling methodWater cooling
Test inventorPower module4th generation SiC MOSFET 1200V/400A
Switching frequency10kHz
Cooling methodWater cooling
Cooling water circulation deviceCooling temperature range20 to 90deg.C
RefrigerantEthylene glycol aqueous solution

Figure 9 illustrates the control system block diagram. The test motor is driven from the DUT inverter through a 3-phase uvw power line. The test motor is connected to the load motor, and the load motor is controlled by the load torque according to the running resistance calculated from the vehicle parameters, which enables the simulated running experiment with the desired vehicle parameters.

Motor test bench / Control system block diagram

Figure 9. Motor test bench / Control system block diagram

DUT inverter drives PMSM via uvw lines; load motor applies WLTC-based torque profile.

International Standard WLTC Mode Fuel Efficiency Test for Simulated Driving

The Worldwide Harmonized Light Duty Driving Test Cycle (WLTC) is a driving cycle specified in the Worldwide Harmonized Light Vehicles Test Procedure (WLTP). This cycle consists of Low, Middle, High, and Extra-High-speed phases. In Japan, test vehicles are driven in the driving cycle except for the Extra-High phase to measure exhaust emissions and fuel consumption.

Using the mentioned motor test bench, ROHM conducted a driving cost test using 4th Generation SiC MOSFETs and IGBTs in the inverter by inputting the conditions of a simulated WLTC driving cycle.

Figure 10 shows the results of the cost test assuming a C-segment class EV, demonstrating that replacing the conventional IGBTs with 4th generation SiC-MOSFETs can improve the cost in all speed phases of the WLTC driving cycle. The total power cost was improved by about 6% compared to the IGBTs, and by about 10% in the urban mode. For reference, Figure 11 shows a graph of the inverter efficiency map (based on the NT curve, with information on efficiency added). From this result, we can see that the efficiency in the high torque and low RPM range, which is frequently seen in urban driving, has been greatly improved.

Electricity cost test result

Figure 10. Electricity cost test result

4th-gen SiC reduces total electricity cost ~6% vs IGBT (≈10% in urban mode) under WLTC profile.

Inverter efficiency map in WLTC electric cost test

Figure 11. Inverter efficiency map in WLTC electric cost test

Efficiency gains are pronounced in high-torque, low-RPM operation typical of urban driving.

Evaluation of Totem-pole PFC

Totem-pole Power Factor Correction (PFC) is a topology that has attracted a great of attention in recent years as a PFC converter that can target high efficiency. In addition, V2G is being considered worldwide to stabilize the microgrid system and contribute to balancing supply and demand, and bidirectional operation has become important.

Figure 12 illustrates the circuit block diagram. The left leg (S1, S2) is for high frequency switching, and the right leg (S3, S4) is for commercial frequency (low frequency) rectification.

Figure 13 shows the operation diagram by state. During the positive half cycle of the commercial AC, the totem pole low side FET (S2) performs high frequency switching as a boost converter (Figure (a): period D). SiC MOSFETs have a very fast recovery time, and the effect of this power loss is small, so they are a good match for Totem-pole PFC power devices. Next, during the negative half cycle of the commercial AC, the totem-pole high-side FET (S1) acts as a boost converter, switching at high frequency (Figure (c): period D), while S2 acts as a rectifier (Figure (d): periods 1-D). S3 and S4 switch every half cycle of the commercial AC.

Totem-pole PFC block diagram

Figure 12. Totem-pole PFC block diagram

Totem-pole PFC with high-frequency leg (S1/S2) and line-frequency rectifier leg (S3/S4).

Operation diagram by state

Figure 13. Operation diagram by state

Operating states across AC half cycles; HF switching in boost leg, rectification in the other.

To verify the contribution of the 4th Generation SiC MOSFETs to the loss reduction of the Totem-pole PFC, an experiment was conducted using the actual board. Table 3 shows the evaluation conditions of the PFC and the specifications of the SiC devices used. When the output voltage is 400V, a SiC MOSFET with 750V breakdown voltage is matched. In this case, SCT4045DR is used. As result, the measured efficiency is over 98% at 1.5kW half load and 97.6% at 3kW full load.

Table 3. PFC evaluation condition

Input Voltage230VAC
Output Voltage400VDC
Output Power3kW
Inductance L500µH
Switching Frequency650kHz
4th Gen SiC MOSFETSCT4045DR 750V/45 mΩ
3rd Gen SiC MOSFET (as reference)SCT3060AR 650V/60 mΩ

Summary

SiC power semiconductors are key power devices for increasing the convenience and power conversion efficiency in applications where high voltage and high current density are progressing, such as EVs, data centers, base stations, and smart grids. In the 4th Generation SiC MOSFET, the trade-off of the trench structure has been greatly improved, and the normalized on-resistance has been further reduced. The high-speed switching performance and low on-resistance of the 4th Generation SiC MOSFETs will greatly contribute to the improvement of power conversion efficiency.

Learn more about ROHM SiC power semiconductors

 

Download this article in pdf.

Download

Applications

Internet of Things

Internet de las cosas

Artificial Intelligence

Inteligencia artificial

Industrial Automation & Control

Automatización y control industrial

Transportation

Transporte

Healthcare

Healthcare

Robotics

Robótica

Maintenance & Safety

Mantenimiento y seguridad

EV Charging

EV Charging

Further Resources

Calculators & Conversion Charts
Selection Guides and Catalogues
Essential Learning Modules
Tech Spotlights
Design Resources
Engineering Glossary
Technical Support
Parts Finder Tools