Press Releases

Newark Extends NXP Freedom Kinetis E Development Kit Series

Low cost MCUs offer 32-bit processing for electrically harsh environments

April 8, 2014 – CHICAGO – As part of its growing development kit offering, Newark has today announced that it is expanding its NXP Freedom Kinetis E Development Kit range with the new KE0240Z, KE04Z and KE06Z Freedom boards. The KE series is designed to provide a low cost, ARM-based, 5V development platform for increased EMI robustness and motor control applications.

Developed for use in electrically noisy environments, the Kinetis E series features a 6-channel, 16-bit Flextimer optimized for motor control. It also includes eight high drive pins with each supporting 40mA. These features make the kit ideal for cost sensitive projects that require various motor control applications as well as a reduced pin count. Typical examples of these applications could include the development of appliances such as DC fans and BLDC Motors, as well as offline UPS and analog power management systems.

The NXP Freedom KE02, KE04Z and KE06 boards are now available through Newark in North America, Farnell element14 in Europe, and element14 in Asia Pacific. The boards will be priced at $12.95, $12.95 and $14.95, respectively.

Key Features include:

  • Either the KE02 40 MHz, KE04 or KE06 microcontroller
  • Accelerometer
  • Thermistor (KE04Z only)
  • IR
  • CAN Communication (KE06Z only)
  • RGB LED
  • OpenSDA
  • Capacitive touch slider
  • Arduino compatible header footprint

Other features include the system's ARM Cortex-M0+ Core, multiple power modes, 12-Bit ADC analogue peripherals, as well as 16bit Flex timers. The KE series also includes Robust 5V MCUs for harsh environments and offers up to 256B EEPROM with 500K endurance cycles.

  • Discussing the announcement, David Shen, Group CTO at Newark said: "The new KE series represents another valued addition to Newark's extensive offering of more than 7,000 development kits. The product marks a significant step forward in the performance available to those looking to develop within electrically noisy environments. Thanks to the increased EMI robustness, the Kinetis E series will offer a far greater degree of control to designers who are looking to save on costs."
  • "The NXP KE Series is the latest in our ever-expanding range of solutions, offering everything from starter kits to complete development boards, including the newest releases and exclusive bundles."
  • Ends

    About the Premier Farnell Group

    Premier Farnell plc (LSE:pfl) is a global leader in high service distribution of technology products and solutions for electronic system design, production, maintenance and repair. It trades as Farnell element14 in Europe, Newark in North America and element14 across Asia Pacific. With sales last year of £968m, the Group is supported by a global supply chain of more than 3,500 suppliers and an inventory profile developed to anticipate and meet its customers' needs.

    Premier Farnell works with key strategic suppliers to bring to market development kits in a variety of applications, enabling it to support the customer from design concept through to production.

    The latest products, software, services and solutions from trusted supplier partners are all available through 43 local language transactional websites, with customer support provided by degreed engineers. The element14 Community allows buyers and engineers to access a wide range of independent technical information, tools and the latest resources.

    Premier Farnell Key facts

    • Operations in 36 different countries
    • More than 4,300 employees
    • More than 3,500 leading suppliers
    • More than 500,000 products stocked with access to over four million more on demand
    • Leaders in providing information on REACH, Conflict Minerals and EU RoHS legislation

    For more information visit the website at Premier Farnell.

    For news updates from Newark visit:

    For additional information:

    William Polk
    PR and Social Media Manager

    Newark
    773-907-5199
    wpolk@newark.com

    Allison Dreiband
    Walker Sands Communications

    For Newark
    312-648-6010
    allison.dreiband@walkersands.com