New Tektronix handheld THS3000 oscilloscopes now in stock at Newark
CHICAGO, JANUARY 19, 2012
Scope series offers up to 5 GS/s sample rate to bring a new level of measurement precision for portable applications
Leading multi-channel electronics distributor Newark, a business of Premier Farnell (LSE:pfl), announced today it was stocking the new Tektronix THS3000 handheld oscilloscope series designed for debugging, installing and repairing complex electronic systems in both field and lab environments.
In today’s world, engineers are often called upon to measure a variety of signals in variety of settings. For many industrial, power generation or power efficiency applications, measurements can include digital and analog control signals made in conjunction with high voltages and currents and often, these measurements are not only made in the lab but also in the field.
With up to 200 MHz bandwidth and a 5 GS/s sample rate, these scopes are the highest performing handheld oscilloscopes available today. Rugged, but lightweight at 4.8 lbs, they also offer up to seven hours of battery life and four isolated channels for use in even the most demanding conditions.
The THS3000 series and the complete Tektronix offering are available for same-day shipping at www.newark.com/tektronix
Editor’s Note: A high res image of the new THS3000 is available at http://www.ftp-newark.com/pr/Tek.jpg
About Newark
Newark is a high-service distributor of technology products and engineering solutions for electronic system design, maintenance and repair. Bringing together the latest products, services, and development software, all connected to an innovative online engineering community where purchasers and engineers can access peers and experts, a wide range of independent technical information and helpful tools. Whether researching a new technology, designing an electronic product, or looking for parts to repair an existing system, Newark is the trusted source to find the answers and parts they need to keep projects on the fast track, right from the start.
Newark is the operating business of Premier Farnell plc (LSE:pfl) in North America and Mexico.
For news updates from Newark visit:
- Premier Farnell Media Centre – www.premierfarnell.com/media-centre/
- Twitter- @element14news | YouTube- element14 | Facebook- www.facebook.com/element14page
- Email: pressoffice@premierfarnell.com
Newark Press Contact
Janice Fleisher
jfleisher@newark.com
773.907.5941