August 2012

On-August Articles

Products & Solutions for Harsh Environments

  • Radial Fin Extruded LED Heat Sinks White Paper

    Continued growth of BRIDGELUX LED lighting products has created a very real need for design and usage guidelines aimed specifically at helping engineers and designers select heat sink products based on both space constraints and operating parameters

    Read the article courtesy of Wakefield

  • Mezalok Connectors: High-Reliability XMC Mezzanine Connector

    Please sUsing proven Mini-Box contacts, compliant solder tails, and an anti-stubbing design, the new Mezalok connectors offer excellent mechanical and thermal cycling stability and footprint compatibility with existing XMC board layouts. ee the full range of Wakefield's standard Thermal Management products by product family, series and most common applications.

    Read the article courtesy of Te-Connectivity
  • Finding faults with voice and data communications

    For locating faults rapidly on voice and data communications installations, a time domain reflectometer (TDR) is likely an invaluable tool. Yet, all too often, TDRs fail to live up to their potential, largely as a result of the limitations inherent in older instruments.The latest generation of TDRs has effectively removed these limitations, making the new instruments more useful – and easier to use – than ever.

    Read the article courtesy of Megger

  • BLACK BOX Ethernet in Harsh Environments

    Ethernet is the most prevalent LAN application worldwide, offering the benefits of standardization, low-cost components, and high-performance switching technology. It's easy to configure and install.

    Read the article courtesy of Black-Box
  • BLACK BOX Power over Ethernet in Industrial Applications

    The Power over Ethernet (PoE) standard, which was adopted in June 2003, enables users to power devices over Ethernet cabling. It was originally developed to provide both power and networking capability in areas where it was previously cost prohibitive or physically impossible to run electrical wiring. PoE has contributed to VoIP and wireless market growth because it simplifies the RF survey task: Access points can be easily moved because the requirement of locally-accessible AC power is removed.

    Read the article courtesy of Black-Box
  • Top 10 Issues to Consider when Specifying an Enclosure for Harsh Environments

    The use of LEDs is finding its way into a myriad of electrical lighting and electronics equipment, some of which were not even imaginable a few year ago.

    Read the article courtesy of AMP Hexseal
  • Burn-in Testing Techniques for Switching Power Supplies

    On a bright, sunny day, the sun's rays give off approximately 1000 watts of energy per square meter of the Earth's surface

    Read the article courtesy of Keithley
  • Power Quality Solutions For the Machine Shop

    While some machine failures are due to faulty equipment a vast majority of failures can be attributed to the quality of power supplied to the machine.

    Read the article courtesy of Sola-HD
  • Ethernet Cable for Industrial Environments

    A high demand exists in the industrial environment for the Ethernet family of computer network technologies for automation and process control.

    Read the article courtesy of Alpha-Wire
  • Evaluating Critical VFD Cable Parameters

    This paper examines the motor-supply cable's impact on VFDs and surrounding equipment. Included are some fundamental guidelines for their installation and design.

    Read the article courtesy of Belden
  • Troubleshooting Load Cell Applications using Agilent Wireless Connectivity Solution

    Troubleshooting a scalefitted with more than one load cell to detect defective cells is always a tedious procedure. Multiple load cells also make troubleshooting harder.

    Read the article courtesy of Agilent
  • Choosing the Right Conformal Coating

    Read the article courtesy of Techsparay
  • Ohmite's 14984 series High Current Round Edge Resistors

    These high current round edgewound resistors handle a variety of harsh environment applications including dynamic braking, loadbanks, motor starting, and plugging.

    Read the article courtesy of Ohmite
  • Corrosion & Harsh Environment Protection

    Save corrosion from eating away at your business…Solutions from T&B

    Read the article courtesy of Thomas-betts
  • Weather the Iraqi Heat

    Technology at work in extreme heat

    Read the article courtesy of Fluke
  • Smart Rack NEMA 12-Rated

    Industrial SmartRack ideal for harsh working environments

    Read the article courtesy of Tripplite
  • Smart Rack NEMA 12-Rated

    Video of Industrial SmartRack ideal for harsh working environments

    Read the article courtesy of Tripplite
  • Fluke 28-II DMM for Harsh Enviornments

    Video - Fluke 28-II DMM for Harsh Enviornments

    Read the article courtesy of Fluke
  • Fluke Scope Meters in Harsh Enviornments

    Video - Fluke Scopemeters in use at Large End-User

    Read the article courtesy of Fluke
  • Understanding Hazardous and Explosion-Protection Environments

    Explosions occur when a mixture of oxygen and explosive substances develop into explosive gases. When the concentration of a substance in air is within the lower and upper explosive limits the mixture can be ignited. To prevent an explosion one of three prerequisites must be eliminated. Making equipment ignition free and safe to install in an explosive environment is one solution.

    Read the article courtesy of Patlite