New to Newark/element14? Start here
2013/05/21
 
 
 

August 2012

Products & Solutions for Harsh Environments

On-demand Articles

Radial Fin Extruded LED Heat Sinks White Paper

Continued growth of BRIDGELUX LED lighting products has created a very real need for design and usage guidelines aimed specifically at helping engineers and designers select heat sink products based on both space constraints and operating parameters

Read article

Article courtesy of
Wakefield


Mezalok Connectors: High-Reliability XMC Mezzanine Connector

Please sUsing proven Mini-Box contacts, compliant solder tails, and an anti-stubbing design, the new Mezalok connectors offer excellent mechanical and thermal cycling stability and footprint compatibility with existing XMC board layouts. ee the full range of Wakefield's standard Thermal Management products by product family, series and most common applications.

Read article

Article courtesy of
Te-Connectivity


Finding faults with voice and data communications

For locating faults rapidly on voice and data communications installations, a time domain reflectometer (TDR) is likely an invaluable tool. Yet, all too often, TDRs fail to live up to their potential, largely as a result of the limitations inherent in older instruments.The latest generation of TDRs has effectively removed these limitations, making the new instruments more useful – and easier to use – than ever.

Read article

Article courtesy of
Megger


BLACK BOX Ethernet in Harsh Environments

Ethernet is the most prevalent LAN application worldwide, offering the benefits of standardization, low-cost components, and high-performance switching technology. It's easy to configure and install.

Read article

Article courtesy of
Black-Box


BLACK BOX Power over Ethernet in Industrial Applications

The Power over Ethernet (PoE) standard, which was adopted in June 2003, enables users to power devices over Ethernet cabling. It was originally developed to provide both power and networking capability in areas where it was previously cost prohibitive or physically impossible to run electrical wiring. PoE has contributed to VoIP and wireless market growth because it simplifies the RF survey task: Access points can be easily moved because the requirement of locally-accessible AC power is removed.

Read article

Article courtesy of
Black-Box


Top 10 Issues to Consider when Specifying an Enclosure for Harsh Environments

This checklist ensures that you will achieve the best balance between protection and cost.

Read article

Article courtesy of
Bud-Industries


Sealing LED Fixtures & Other Opto Devices

The use of LEDs is finding its way into a myriad of electrical lighting and electronics equipment, some of which were not even imaginable a few year ago.

Read article

Article courtesy of
APM Hexseal


Power Quality Solutions For the Machine Shop

While some machine failures are due to faulty equipment a vast majority of failures can be attributed to the quality of power supplied to the machine.

Read article

Article courtesy of
Sola-HD


Ethernet Cable for Industrial Environments

A high demand exists in the industrial environment for the Ethernet family of computer network technologies for automation and process control.

Read article

Article courtesy of
Alpha-Wire


Evaluating Critical VFD Cable Parameters

This paper examines the motor-supply cable's impact on VFDs and surrounding equipment. Included are some fundamental guidelines for their installation and design.

Read article

Article courtesy of
Belden


Soak up Facts on Sorbents

Nearly every facility needs absorbent material for cleaning up liquid messes. Slow leaks and major spills are inevitable, and prompt, thorough clean-up is essential to maintaining a safe, clean work environment.

Read article

Article courtesy of
3M


Troubleshooting Load Cell Applications using Agilent Wireless Connectivity Solution

Troubleshooting a scalefitted with more than one load cell to detect defective cells is always a tedious procedure. Multiple load cells also make troubleshooting harder.

Read article

Article courtesy of
Agilent


Ohmite's 14984 series High Current Round Edge Resistors

These high current round edgewound resistors handle a variety of harsh environment applications including dynamic braking, loadbanks, motor starting, and plugging .

Read article

Article courtesy of
Ohmite


Ohmite's Rugged 280 Series Corrib® Vitreous Enamel Power Resistors

These large, heavy-duty resistors are designed to withstand frequent start-stop cycles characteristic of motor starting, dynamic braking and other similar applications.

Read article

Article courtesy of
Ohmite


Corrosion & Harsh Environment Protection

Save corrosion from eating away at your business…Solutions from T&B

Read article

Article courtesy of
Thomas-betts


Weather the Iraqi Heat

Technology at work in extreme heat

Read article

Article courtesy of
Fluke


Smart Rack NEMA 12-Rated

Industrial SmartRack ideal for harsh working environments

Read article

Article courtesy of
Tripplite


Smart Rack NEMA 12-Rated

Video of Industrial SmartRack ideal for harsh working environments

Read article

Article courtesy of
Tripplite


Fluke 28-II DMM for Harsh Enviornments

Video - Fluke 28-II DMM for Harsh Enviornments

Read article

Article courtesy of
Fluke


Fluke Scope Meters in Harsh Enviornments

Video - Fluke Scopemeters in use at Large End-User

Read article

Article courtesy of
Fluke


Understanding Hazardous and Explosion-Protection Environments

Explosions occur when a mixture of oxygen and explosive substances develop into explosive gases. When the concentration of a substance in air is within the lower and upper explosive limits the mixture can be ignited. To prevent an explosion one of three prerequisites must be eliminated. Making equipment ignition free and safe to install in an explosive environment is one solution.

Read article

Article courtesy of
Patlite



 
 

Featured Product

Schneider Electric

XTRA-GUARD Industrial Ethernet CAT 5e Shielded and Unschielded Multipair Cable

See more»

Schneider Electric

TURBO-COAT Acrylic Conformal Coating

See more»

Schneider Electric

AGILENT TECHNOLOGIES - U1177A - Bluetooth Adapter

See more»


Featured Offers


Agilent Technologies
Get 20% off Microwave HandHeld Spectrum Analyzers from Agilent
Offer ends 08/31/2012
Fluke
SCORE MORE!
BUY a Fluke Tool
GET a FREE GIFT!
Offer ends 12/31/2012
Amphenol
Get In The Game
BUY an Amprobe Tool
GET a FREE GIFT!
Offer ends 12/31 2012