New to Newark/element14? Start here
2013/05/18
 
 
 

On-Demand Solutions | August 2011

On-demand Articles

Harsh environment solutions

Oil rigs, mines, wind farms, and industrial manufacturing facilities are often located in remote,

Read article

Article courtesy of Panduit


Five painless ways to save money and time on your harsh environment purchases

Purchasing products for use in a harsh environment can be a tricky business. The components need to be protected but it is also important not to overkill the protection and waste costs.

Read article

Article courtesy of BUD


Connectors for harsh environments

Circular connectors are finding increased usage in today's interconnected industrial electronic equipment. As a result of this increase in connectorization, there is an ever growing appetite for connectors that can withstand a wide range of use and "abuse".

Read article

Article courtesy of Souriau


Upgrade your facility by practical steps to reduce arc flash

Quantification of the arcflash hazard level and labeling procedures are a major portion of this effort.

Read article

Article courtesy of Eaton


Environmental protection of HMI Components

Electromechanical devices, including switches, keypads, keyboards, pointing devices and other elements such as indicators and alarms, are critical aspects of the human-machine interface (HMI) for controlling equipment and systems.

Read article

Article courtesy of EAO


Understanding degrees of protection - IP Codes

Equipment has to fulfil its functional requirement. But only that is not enough. The equipment has also to be protected against possible external influences and the equipment may not be harmful to the user or operator or to the environment.

Read article

Article courtesy of Eaton


How to specify high performance cables

There is no acceptable level of downtime and no one can afford to replace expensive machinery years before its predicted lifespan—not when profit margins are razor thin and competition is breathing down your neck from all four corners of the world.

Read article

Article courtesy of Alpha Wire


When accuracy is critical

In this era of increasing industry and government standards, the demands on calibration laboratories are growing. Whether it's an in-house cal lab or a field unit, the pressure is on to conduct more calibrations in a short period of time while still maintaining a high degree of accuracy.

Read article

Article courtesy of Pomona


Seven practices to prevent damaging power meters and power sensors

Year after year, a significant number of power sensors are damaged because of users' carelessness or ignorance. Knowing the proper usage and precautions for power sensors and meters would spare you inconvenience and downtime required for repair.

Read article

Article courtesy of Agilent


Embedded design techniques for optimizing control parameters

In the process of optimizing control functions, small adjustments in microcontroller firmware can produce significant improvements in embedded system performance. Coming up with the right values for gains, offsets, delays, hysteresis values and PWM parameters can be time consuming, but using the right tools can speed the process.

Read article

Article courtesy of Tektronix


Test jumpers for nuclear power

When the cost of a human error can easily cost your company millions of dollars or more in lost revenue, minimizing errors is critical. When it also happens to be a nuclear power plant, the stakes are even higher.

Read article

Article courtesy of Pomona


Edwards signaling introduces the 116EXMLED Hazardous Location LED Signa

Introducing the NEW Edwards Signaling 116 LED Hazardous Location Beacon designed for Class 1, Div 1 environments. The new 116EXMLED provides the bright visual indication required when emergencies arise in hazardous industrial and process environments.

Read article

Article courtesy of Edwards Signaling


On-demand Products

Eaton

Eaton Series G Circuit Breakers

See more»

eao

EAO 704 Series 22.5mm Pushbutton Switches and Indicators

See more»

Agilent Technologies

Excellent for motor start, motor run applications.

See more»

Special Offers

Agilent Technologies

Add Wireless LAN to Agilent's 34972A Data Acquisition Unit at No Extra Cost!

See more»

TE Connectivity

Save On Our Huge Selection of Relays & Contactors from TE Connectivity

See more»

Overstock

Overstock Sale!

See more»

 

Online Catalogs