Press Releases
EAO introduces new Series 51 stop switches at Newark element14
Space-saving design sets a new standard in the industry
CHICAGO, MARCH 21, 2012 - Newark element14, the leading distributor of electronic components and engineering solutions in the Americas and a business of Premier Farnell (LSE:pfl), announced today it was the first to stock the new EAO Series 51 Stop Switch, which features a monoblock design with a back panel depth of just 18.8mm—less than the width of a penny and unmatched by any other stop switch in the industry
The space-saving design makes the Series 51 ideal for applications that require exacting ergonomics combined with superior reliability and durability, and is especially well-suited for interfaces that require a visible actuation status, such as medical diagnostic equipment, machinery, and many other space restrictive applications that employ hand-held pendants. Monoblock construction provides fail-safe operation which ultimately increases overall user safety.
The switch is sealed to IP65 standards from the front of the panel, utilizing an industry standard 16 mm mounting hole, and it meets many international standards, including CE, EN 61058-1 and RoHS environmental requirements
The full offering of EAO switches is available for same-day shipping at http://www.newark.com/eao

About Newark/element14
Newark/element14is a high-service distributor of technology products and engineering solutions for electronic system design, maintenance and repair. Bringing together the latest products, services, and development software, all connected to an innovative online engineering community where purchasers and engineers can access peers and experts, a wide range of independent technical information and helpful tools. Whether researching a new technology, designing an electronic product, or looking for parts to repair an existing system, Newark/element14 is the trusted source to find the answers and parts they need to keep projects on the fast track, right from the start.
Newark/element14 is the operating business of Premier Farnell plc (LSE:pfl) in North America and Mexico.
For news updates from Newark element14 visit:
Premier Farnell News Centre – www.premierfarnell.com/premier_farnell/publicrelations/
Twitter - @element14news
YouTube – element14
Facebook – www.facebook.com/element14page
Email: pressoffice@premierfarnell.com
Newark Press Contact
Janice Fleisher
jfleisher@newark.com
773.907.5941
|